Sample Rate

Analysis > FMCW Radar Properties > Time

Specifies the Sample Rate (Hz) at which the FMCW Reference Synchronization and analysis will be performed.

The measurement Sample Rate (Hz) and reported Bandwidth (Hz) values are both directly related to the currently selected measurement acquisition Span (Hz) as follows:

You can alternatively set the desired measurement Bandwidth (Hz) by manually setting the Span (Hz) (Analysis > Frequency), which will also update the Sample Rate (Hz) value used by the relationship given above.