Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic Go to Topic

Reference Synchronization Tab

Menu Path: Analysis > FMCW Radar Properties

The Reference Synchronization properties allow you to specify an appropriate FMCW region synchronization method to use for achieving reference time alignment to each of the individual Linear FM Frequency Modulation (LFM) modulation regions contained within the measured signal, along with the associated synchronization method setup parameters.

Additionally you can specify the desired FM Filter Bandwidth applied to the measured signal, which can affect both FMCW reference synchronization and analysis.

The choices that appear depend on the type of Region Synchronization selected, as shown in the illustrations below.
Region Synchronization Set to
Automatic
Region Synchronization Set To
Sync to Manual Reference or Triggered

See Also

Preset FMCW Radar Measurement

Region Synchronization

Reference Data Selection

Auto Detect Setup

Max Region FM Slope Deviation

Reference Region Count

First Region FM Slope

Manual Reference Description

FM Filter Bandwidth