Time Metrics
Menu Path:
Menu Path:
The Region Table, Cumulative Statistics Table, and Current Statistics Table allow you to display the following Time metrics:
- Time Start (sec)
- Time Start (in seconds), reports the relative timing to the start of each detected LFM region's user defined analysis time samples. Note that this result is affected if Exclude During Analysis is used to exclude time samples.
- The Time Start relative definition can be controlled by Time Values Are Relative To, with valid choices of:
- First Region
- Report per region time values relative to first detected region start time (i.e. relative to reported Region 1 Time Start (s) within Region Table results).
- Trigger
- Report per region time values relative to acquisition trigger event time, as determined by user configured Input Trigger properties.
- First Region
- Default visibility: ON
- Time Length (sec)
- Time Length in seconds, reports the analysis time interval over which each LFM region's results are measured starting from the reported Time Start (s) value, as determined by user defined analysis time samples. Note that this result is affected if Exclude During Analysis is used to exclude time samples.
- Default visibility: ON