Acquisition Time
Menu Path:
Acquisition Time reports un-synchronized measured signal acquisition IQ samples over time.
When Time Values Are Relative To is set to First Region, X-axis time values are displayed relative to first detected region Time Start (s) value.
When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to acquisition trigger event occurrence.
See Also