Phase Meas Time
Menu Path:
Phase Meas Time reports region-synchronized measured signal phase samples over time in degree.
When Time Values Are Relative To is set to First Region, X-axis time values are displayed relative to the first detected region Time Start (s) value. When the property Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to the acquisition trigger event.
When Compensate Phase Results for Frequency Offset is enabled, the reported per region measured and reference synchronized phase trace results are automatically compensated for each specific regions measured mean frequency offset from the current Center Frequency value.
The Inst Phase Meas Time is a non-averaged version of Phase Meas Time.
Valid trace Format selections are:
- Real