Phase Ref Time
Menu Path:
Phase Ref Time reports pulse -synchronized reference signal, unwrapped-phase samples over time in degree.
When Time Values Are Relative To is set to First Region, X-axis time values are displayed relative to the first detected region Time Start (s) value. When the property Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to the acquisition trigger event occurrence.
When Compensate Phase Results for Frequency Offset is enabled, the reported per region measured and reference synchronized phase trace results are automatically compensated for each specific regions measured mean frequency offset from the current Center Frequency value.
Valid trace Format selections are:
- Real