Trace Layout Submenu
From the
submenu you can choose one of several types of trace layouts, specify a custom layout, or revert to a previous trace layout.You can also access the in the Trace Toolbar.
Trace Layouts
You can control which traces are displayed in the layouts by selecting from the View Trace menus.
The following table describes each layout. When there are more visible traces than will fit in the trace layout, extra traces are distributed evenly in the layout as extra tabs. When there are fewer visible traces than the selected trace layout needs, the remaining trace windows will be added.
Trace Layout |
Description |
---|---|
Previous Layout |
Reverts to the previous trace layout. You can revert to any previous layout in the current VSA session. |
Single |
All visible traces are placed in a single tab group. |
Stack N |
N evenly spaced trace windows are stacked on each other. |
Grid NxM |
A grid of trace windows with N rows and M columns. |
Custom |
Brings up the Custom Layout dialog that contains parameters for configuring a custom trace layout. |
Tile Visible |
Automatically creates a custom trace layout based on all currently open traces. Screen space is allocated as evenly as possible, and traces that are hidden (tabbed) are promoted to have their own space. |
Manually configuring trace window layout
You can also use the docking window features of the 89600 VSA to arrange the traces in a custom manner not provided by the Using the Docking Window Manager topic for more information.
commands. See theSee Also