Trace/Block Diagram Toolbar
The trace/block diagram toolbar contains controls for configuring the traces used in a measurement and toggling the visibility of the Block Diagram.
Active Trace |
Displays the letter designation of the active (currently selected) trace. |
|
Trace Layout |
Click to open a drop-down menu of predefined trace layouts, or create a custom layout. This button is a shortcut to the Window > Trace Layout menu. Tile Visible automatically creates a custom trace layout based on all currently open traces. Screen space is allocated as evenly as possible, and traces that are hidden (tabbed) are promoted to have their own space. |
|
Block Diagram |
(Main VSA toolbar only) Click to toggle the visibility of the Block Diagram. This button is a shortcut to the Window > Block Diagram menu selection. |
Any trace data, trace format, scale, or marker selections made apply only to the active trace. When a trace is saved or copied, only the active trace is saved or copied.
See Also