89600 VSA Application Window Illustration
This illustration shows the default setup of the 89600 VSA main window. This illustration identifies where the common elements and features of the VSA application user interface are located.
For more information about menu items and toolbars, see the Default Menus, Standard Toolbars, and Popup Menus topics in the Reference.
See Also