Custom Layout Dialog Box
The dialog box allows you to perform a trace layout with the desired number of rows and columns. The following are the available parameters and descriptions.
- - number of rows in the layout
- - number of columns in the layout
- - when selected, trace lettering increases downwards from the top-left trace. When cleared, trace lettering increases to the right from the top-left trace.
- - when selected, trace windows are added to ensure the specified x layout is filled. Otherwise the VSA places the trace windows in the manner specified by until there are no more traces to place.
- - when selected, the VSA hides any extra traces once the specified x layout is filled. When cleared, the VSA begins at the top-left trace window and continues in the manner specified by , adding the remaining traces as tabs.
See Also