Full Scale (X Scale)
The check box determines how much of the trace data is shown. When the check box is selected, all points are shown on the trace. When the box is cleared, Left Reference and Right Reference determine what part of the trace data is shown.
The check box is cleared when the X-axis scale is changed. The X-axis scale can be changed by adjusting the /trace hotspots or by using the Select Area tool and clicking either or . The check box is also cleared when trace data is recalled that is not full scale.
To quickly reset the x-axis to full scale: Right click in the x-axis annotation area of a trace (below the trace grid) and select .
See Also