Digital Demod Tab (Trace)
The
tab in adjusts parameters that affect how demodulated data is displayed. The following trace parameters can be adjusted:- Trace controls: At the top of the tab are controls for selecting, adding, and removing traces.
Ideal State: chooses a circle or cross (or none) to indicate the location of ideal states. State size can be adjusted to change the size of the ideal states (in % EVM).
:
Select the check box to make the trace visible on the display; clear the check box to remove the trace from the display. When the trace is enabled, the following parameters can be set for the trace:
- Code Order: selectsW-CDMA or cdma2000 Code Domain Power display. or code order for the
- Eye Length: determines the length of eye or trellis diagrams.
- Filtered Channel Types: allows filtering of trace data by physical channel type when multiple channels are present in a trace.
- Filtered SubSegments: allows filtering of layers and subsegments in a trace when multiple layers, subsegments, or a combination are present in a trace.
- Frequency Unit: selects the x or z-axis frequency units that are applied to marker readouts for trace data results that use carrier information.
- check box: shows the average line which overlays OFDM subcarrier traces when the check box is selected. Disables the average line when cleared. The 2D average line shows the average of all values on the Z-axis for each X-axis location.
- Symbol Table Bit Order: sets the bit order of hex values in symbol tables to MSB first or LSB first or auto.
- Symbol Table Format: selects binary or hexadecimal data for the symbol table.
- Symbol Shape: selects a bars or dots (or none) to indicate symbol locations.
- Time Unit: selects symbols or seconds as the time unit for time traces.
See Also