Raw Main Time (Trace Data)
Main Time with the following exceptions:
is the raw data read from the input hardware or playback file. is similar to- The data has not had time corrections applied, so the trace shows a "CAL?" trace indicator.
- The data has not gone through the VSA's software resampling filters, so is generally not sampled at the specified sample rate.
- The data has a wider bandwidth than the measurement span would indicate.
data is useful in the following situations:
- When Channel, IF Magnitude or Magnitude trigger types are used, the input hardware detects the trigger so sometimes gives a better indication of what caused the trigger.
- When a recording is played back, the measurement data shows exactly the samples that are saved in the recording, with no filtering applied or settling removed.