User Defined Preset Context Type
The context type allows you to cache a measurement's setup for later use, without having to save a setup file. Cached measurement setups have a limited lifetime, reflecting the lifetime of the current instance of VSA. However, during that lifetime, they can be applied to a measurement as many times as desired. This allows for expedient setup switching without having to do file management.
Cache Measurement Setup - Copies the current measurement's state into a local cache.
Apply Cached Setup - Applies the cached setup to the current measurement.
See Also