Playback tab (Recording)
The Playback tab sets parameters that control how a recording is played.
- and show the playback's start and stop times. By default, the start time is zero and the stop time is the end of the time record. Both values can be reset by clicking the button.
- The button resets Start Time and Stop Time to their default values.
- controls playback operation when the recording ends. Selecting this box causes the recording to play continuously, looping to the beginning when it reaches the end. When the check box is cleared, playback stops when the recording ends.
See Also