Using Fixed Equalization

To enable fixed equalization:

  1. Choose the Measurement Channel to which fixed equalization is to be applied.

  2. Select the Fixed Equalization check box (Acquisition > User Corrections > Fixed Equalization or Acquisition > Playback User Corrections > Fixed Equalization).

  3. Choose a register which has a previously saved frequency-domain data. This data defines the response of the equalizer FIR Finite Impulse Response filter.

  4. Specify whether or not the equalization should be inverted.

See Also

Fixed Equalization

About Fixed Equalization