Gate Enabled (Gate Trigger)
Enables gating.
Gating uses the gate length to specify the acquisition length at each gate occurrence and therefore the behavior is different when gating is enabled than when it is disabled even when the Gate Style is set to Free Run.
See Also