Length (Gate Trigger)
(Power Spectrum based Input Domain Power Spectrum measurements only)
Sets the length of time in seconds for the acquisition data to acquire and use for a step in the spectrum once the gate trigger condition occurs. The Video Bandwidth normally influences the length of the acquired data when gating is not used. But, when gating is used then the gate Length parameter has priority and the Video Bandwidth parameter will be treated as the maximum desired Video Bandwidth.
See Also