Peak Hold (Gate Trigger)
The peak hold function is located before combining high and low side mixing when using double acquisition conversion for image suppression (which is also before the detectors). It can be enabled when not using double acquisition conversion. See the Achieving Excellent Spectrum Analysis Results Using Innovative Noise, Image and Spur-Suppression Techniques application note for more information on when this may be useful.
See Also