IF Mag Trigger Style (Trigger)
The trigger style is available when using zoomed (real and imaginary) time data. The trigger only triggers when the signal is within the specified frequency span, as shown in the following block diagram:

The trigger is usually used with amplitude modulated (AM Amplitude Modulation - CW modulation using amplitude variation in proportion to the amplitude of the modulating signal. Usually taken as DSB-LC for commercial broadcast transmissions and DSB-SC for multiplexed systems.) or burst signals. This trigger style triggers the VSA under the following conditions:
-
the input signal is within the current span
-
the input signal is varying in amplitude
-
the trigger conditions are met.
The trigger conditions that can be specified are level, slope, delay, and hold-off.
With, the magnitude of the IF signal must vary to trigger the VSA. The magnitude of the IF signal varies when the input signal switches on and off or if the input signal is AM modulated.
Trigger is often used with . If using an IF burst to trigger the VSA and the IF burst contains more than one valid trigger edge, use trigger to ignore all but the first trigger edge.
Viewing the IF Signal
The following steps show how to view the trigger signal. This is useful for determining the best values for trigger level and slope.
- Make sure and are off.
- Click :
- In the box, select .
- In the box, set the center frequency to the frequency of the carrier.
- Click . In the box, select .
- Click and select a time domain display ().
There are some considerations to be aware of when viewing in the time domain. See below for details.
Considerations
- With , the magnitude of the IF signal must vary to trigger the VSA. The magnitude of the IF signal varies when the input signal switches on and off or if the input signal is AM modulated.
- Trigger conditions (, and ) must be met to trigger the VSA.
- Use trigger if there are multiple, valid trigger signals within the IF signal. With trigger , configure the VSA to ignore extra trigger signals.
- To get an accurate time-domain display of the trigger signal, make sure the input signal is within the specified frequency span.
- If the DC level is too high, the DC level introduces a second waveform that makes the trigger signal look like a mixed signal. This problem is most apparent with DC coupling, but may also be apparent with AC coupling.
- To avoid problems caused by DC level, set the stop frequency high enough that DC is out of band. Usually, setting the stop frequency to 0.1´ span is sufficient; however, it may need to be set as high as 0.3´ span.
See Also