Ref BW (ACP Marker Properties)
: 1 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second.
The parameter specifies the ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power. measurement's reference channel bandwidth.
The reference channel's center frequency is determined by the VSA's center frequency.
See Also