RRC Shape (Reference channel)
: cleared
Use the reference channel parameter to control the Root Raised Cosine shape of the ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power. marker's reference channel.
-
Selected: Enables the Root Raised Cosine shape of the ACP reference channel marker for the active trace.
-
Cleared: Disables the Root Raised Cosine shape of the ACP reference channel marker.
The reference channel's checkbox must be selected to activate the checkbox.
The parameter specifies an alpha value of the Root Raised Cosine shape for the ACP marker's reference channel. This parameter is only available when the parameter has been selected. The default for is 0.
When the reference channel's parameter is set to zero, the filter is effectively disabled for the reference channel. This applies the Root Raised Cosine shape to the adjacent channels but not the reference channel.
See Also