Polar Format (Markers)
specifies the format of marker readouts for markers on traces with a polar trace format (I-Q or Const). The available selections are as follows:
- - shows the magnitude and phase of the marker position (for example, .995 mVrms -45 deg)
- - shows the real and imaginary part of the marker position (for example, .705 m -.705 m)
Switching between the two polar formats has no effect for markers on traces whose trace format non-polar.
See Also