Measurement Channel (Frequency)

Menu Path: Analysis > Frequency

Measurement Channel selects the measurement channel/channels' settings to change when you edit the parameters on the Frequency tab. The button choices include All and the number of channels set in Input Channels.

For more information, see Measurement Channel in Analog Input Properties.

See Also

Frequency Tab

About Channels