ResBW Mode (ResBW)
The choice of resolution-bandwidth mode in conjunction with the choice of resolution-bandwidth coupling mode affects both resolution and measurement speed.
Keysight 89600 VSA offers two levels of flexibility in selecting a resolution bandwidth setting: and :
- mode is more restrictive than mode. In mode, the VSA always sets the resolution bandwidth using the pattern { ..., 1, 3, 10, 30, 100, 300, ... } MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. (emulating many existing spectrum analyzers).
- mode allows an arbitrary resolution bandwidth setting. The choice of bandwidth mode in conjunction with the choice of affects both resolution and measurement speed. To get the best resolution-to-speed tradeoff when changing the measurement span, specify ResBW coupling and ResBW mode.
See Also