ResBW Coupling (ResBW)
ResBW determines how resolution bandwidth (ResBW) changes when you change the frequency span. The selections are as follows:
-
coupling: This coupling chooses the narrowest ResBW value that is consistent with the Span, ResBW mode, Window Type, and number of frequency points. (ResBW coupling is only available in Manual Frequency Points mode.) This ResBW that provides the best compromise between measurement speed and frequency resolution when you change the frequency span.
-
coupling: This coupling attempts to maintain the same ResBW-to-span ratio when the frequency span is changed (see Offset coupling below for details).
- coupling: This coupling does not
change ResBW when the frequency span is changed. coupling is automatically
selected when the value of Main
Time Length is changed or when time gating is turned on. This is necessary to maintain
the selected value of or .
When Time Gating is enabled, only coupling is available. This is because the ResBW is directly dependent on the length of the time record used to compute spectral traces and Time Gating effectively fixes the time length (and thus ).
The value of resolution bandwidth depends on the selected and the Main or Gate Time Length. The effect of selecting or coupling is to cause resolution bandwidth to depend on frequency span as well.
Offset coupling
The current resolution bandwidth can easily be overridden by manually entering a setting of your own. When ResBW is manually specified, the VSA will attempt to maintain the ResBW/Span ratio when the Span is changed. This is called offset coupling.
For example, a change to a narrower resolution bandwidth than the default ( coupling), will cause the VSA to switch to coupling and maintain a narrower-than-normal resolution bandwidth for subsequent spans. Offset coupling causes the frequency spectrum to appear the same when the span is changed.
When ResBW Mode is arbitrary, the ResBW/Span ratio is exactly maintained. When ResBW is 1-3-10, the ratio cannot be exactly maintained because ResBW is rounded up to the next 1-3-10 value.
See Also