Auto Time Resolution (Time)
Cleared
For the VSA to determine the best , and for a given Time Length, it is recommended that be enabled rather than . provides the most flexibility in specifying a or Time Length for a given and .
The parameter remains available for software backwards compatibility. Selecting the check box causes the VSA to automatically reduce or increase the frequency span when the value of main time length exceeds that allowed by the current span. This is useful to set main length and let the VSA select the time resolution, that is, let the VSA choose the span.
See Also