Detect PRI for Fast-Time (Time vs. Time)
Detect PRI for Fast-Time sets the Fast-Time slice length based on the pulse repetition interval (PRI) of the signal. Setting the Fast-Time length to the PRI ensures that pulses are stacked and aligned vertically in the Time vs. Time Heatmap. This is important for visualizing deviations in the pulses (like a jammer pulse), especially when they stand out as patterns in the heatmap.
This button estimates the PRI leveraging a burst detection method that finds the amplitude bursts in the time domain signal, and averaging the repetition interval of the bursts to get the best possible Fast-Time Length.
See Also