Max Analysis Points (Time vs. Time)
Max Analysis Points represents an upper bound where analysis stops after exceeding this bound. Data will stop being processed beyond the max analysis point sample, and the rest of the data seen in the heatmap will be 0s. This can be increased or decreased, but increasing this could lead to a slow down in the VSA measurement.
When Auto is selected (default = selected), the max analysis points value is automatically determined as a reasonable value for all types of hardware. This may be extended based on the computer processing speed and memory depth.
Max Analysis Duration displays a read-only value to help customer understand what Max Analysis Points equates to in time.
See Also