Center (Digital Input)
represents the center frequency associated with complex digital data coming from the Logic Analyzer. The default value is 0 Hz. If digital data represents complex data that has been converted to an intermediate frequency (IF) by a digital mixer, enter the IF here. If the digital data is real, the property is ignored.
The and Sample Rate properties establish the limits for the Center Frequency of a measurement as follows:
(real data)
Minimum Center Frequency = 0
Maximum Center Frequency = Sample Rate / 2.56
(complex data)
Minimum Center Frequency = Center - Sample Rate / 2.56
Maximum Center Frequency = Center + Sample Rate / 2.56
The of the measurement may be set to any value within these limits. The VSA mixes the incoming data with a complex local oscillator to make the change.
Whenever the or properties are changed, the of the measurement is reset to equal the property and the Span is reset to the maximum value determined by the .
is the same for all channels. Setting the value for any channel sets the same value on all other channels.
See Also