About Digital Input Properties

The Digital Input Properties configure how the 89600 VSA software interprets data from a Logic Analyzer. The Digital Input Properties are located on the Digital tab of the Input dialog box (Acquisition > Digital).

The Digital tab is only available when a Logic Analyzer is a Logical Instrument in the Current Analyzer Configuration.

The Digital tab contains a Digital Channel selection and three groups of digital data properties:

Some properties are channel independent and their values are applied to all channels regardless of the Digital Channel selection. For these properties Digital Channel is ignored. Other properties are channel dependent and their values are applied to the specific channel specified by Digital Channel.

See Also

Input Menu

About Logic Analyzers with 89600 VSA Software