Scale (Digital Input)
Logic Analyzer data buses consist of several digital channels grouped together in a specified order and given a name. Each sample of an n-bit bus is interpreted by the 89600 VSA as a signed integer. The full range of integer values taken on by a bus is mapped to the interval (-1, +1) times its associated factor, whenever it represents a real or imaginary number. If it represents phase, it is mapped to (-p, +p) times its factor.
The property is channel specific; it can be set individually for each Digital Channel.
See Also