Tool Name (Digital Input)
The selects the Logic Analyzer software Tool for the chosen input module.
In the Logic Analyzer configuration, hardware modules can be connected to software Tools that further transform the data. The 89600 VSA software can analyze data from selected Logic Analyzer software Tools. Currently the only supported Tool is the "Signal Extractor" tool (Logic Analyzer application version 3.50 and later). The Signal Extractor provides flexible de-serialization of serial data or serialization of several parallel buses into one bus.
When a is selected, the drop down is updated with a list of the Tools available at the output of the selected module. To assign a Tool to a channel, select the and then select the . Any Tool can be assigned any channel or “None“ can be selected to analyze data directly from the module. The default selection is “None” and the is set to the default whenever the Module Name is changed.
When the changes for a channel, the property is updated to the currently available bus names.
The VSA will only use Tools that receive input from hardware modules and not Tools connected to other Tools.
See Also