Preset Measurement

Presets the specified measurement to a Vector measurement.

The existing measurement trace layout is reset such that there are two traces per input channel: Spectrum and Main Time. The traces are also moved into the VSA Main Window.

Other measurements are unaffected except when you preset one of several measurements that share hardware.

In this case, the preset operation may cause the other measurements settings to be limited due to hardware constraints as the preset measurement's settings are changed to the defaults for the Vector measurement.

See Also

Save Measurement

Preset Setup

About Preset