Aux IF Frequency (External Mixer)

Menu Path: Acquisition > External Mixer

Aux IF Frequency sets the frequency of the converted signal to match the frequency of the auxiliary device when Mixer Paths is set to Aux Equipment.

 Range: 0.0 Hz to 4.0 GHz Gigahertz: A frequency measurement which equals one billion hertz. (for M1971E-Band Waveguide Harmonic Mixer)

See Also

Acquisition Menu

External Mixer