About External Mixers (Acquisition)

The External Mixer tab in the Input dialog is used to configure an external mixer attached to the LO/IF port of an X-Series Signal Analyzer.

Here is a list of the properties shown in the External Mixer tab:

The External Mixer tab is modeled after the external mixer settings in the X-Series Analyzer. For more information, see the help for the external mixer topics located in the Input/Output > External Mixer section in the X-Series Help.

Amplitude Corrections

To correct for amplitude variations of the external mixer, you can use the corrections defined in the X-Series Analyzer by setting the Instrument User Corrections parameter to On or by defining an RF Filter with User Corrections.

The amplitude corrections supplied by the smart mixer to the X-Series Analyzer will be applied to the time data sent to the VSA.

See Also

Acquisition Menu

Instrument User Corrections (Input Extension)