Input Attenuation (External Mixer)
0 dB to 26 dB
sets the attenuation of the attenuator at the input of the external mixer. This property is supported by the V3050A Signal Analyzer Frequency Extender. It is displayed on the External Mixer panel only when supported by the external mixer.
See Also