USB Mixer Status (External Mixer)
The status area shows the status of a smart mixer plugged into a USB port on the X-Series Signal Analyzer as well as the smart mixer's and .
When a smart mixer is plugged in, a status message "USB Mixer detected" will be shown and the Mixer Selection will be changed to the smart mixer.
If the smart mixer is then unplugged, the will still show the smart mixer, but the status message "USB Mixer not detected" will be shown.
When a (non-USB) mixer is selected from the menu, the USB Mixer status will be cleared.
See Also