About Limits Marker (Markers)

Limit tests can be created to compare trace data to your defined limits and indicate a pass or fail condition. A limit test is a collection of limit lines which define the acceptable area of the trace.

A limit test can be applied to the active trace by selecting the limit test from the Limits Tab in the Markers dialog box.

Limit tests can be created using the Limit Tests dialog. Once limit tests have been created, they can be edited using the Edit... shortcut button in Trace > Calculation > Limit Tests Tab.

See Also

Limits Tab (Limits)

About Limit Lines (Limits)

Limit Test Editor (Limits)