Visible (Markers)
Select Visible check box to change the visibility of the active marker.
Normal and delta markers are shown on a trace as a diamond directly above the point the marker is pointing to. Fixed markers are shown as an 'X' shape where the center of the 'X' indicates the marker position.
When a marker is visible and active, the VSA shows a marker readout above the trace grid on the right. Marker values for all visible markers are also shown in the Markers Window. Marker readouts in the contain active hotspots that can be used to specify a new position for the marker.
See Managing Markers for information on adding and removing markers from traces.
See Also