Minimum and Maximum ResBW
ResBW depends on the window type and the time length (main time length, gate time length, or trace length for digital demods).
For non-digital demods, the minimum ResBW depends on the maximum time length. For digital demods, ResBW cannot be set directly but is determined by the length of the trace.
The maximum ResBW is limited to 0.3 * Span.
See Also