Reference Position (Y Scale)
100%
for Log Mag, Lin Mag, and Log Mag(lin)
50% for other trace formats
0% to 100%
1% increments
determines the position of the Reference Line for the active trace.
The reference line is shown only if the check box is selected.
For more details, see Reference Level.