Delay (User Correction, Playback User Correction)

Menu Path: Acquisition > User Correction

Acquisition > Playback User Correction

 Default: 0 sec

Delay is relative to the trigger. Trigger delay can also be used to compensate for the delay of external devices.

Adjusting an input channel's delay with trigger delay has the same effect as adjusting the channel's delay with user correction. However, trigger delay is a coarser adjustment.

The frequency span determines the delay resolution for trigger delay. Frequency span does not affect the delay resolution for user correction. Thus, the current frequency span may only set the trigger delay in nanoseconds, whereas user correction sets the delay in picoseconds.

See Also

Amplifier/Attenuator

About User Correction

About Playback User Correction