IF Center Frequency (User Correction)

Menu Path: Acquisition > User Correction

The IF Center Frequency for the external downconverter can be entered in this text box. This is the frequency at which a sine wave signal would appear at the output of the external downconverter if a sine wave is input at the RF Center Frequency.

See Also

Frequency Converter