RIF-RMARKER (802.15.4 HRP UWB)
is the location of the first chip in the first RIF after the SFD Start frame delimiter. When playing back from a recording, RIF-RMARKER is expressed relative to the beginning of the recording. When acquiring data from hardware, RIF-RMARKER is expressed relative to the trigger point.
See Also