RIF Avg Pulse Amplitude (802.15.4 HRP UWB)
is the average pulse amplitude level for the RIF part of the frame, expressed in dB relative to the average SHR pulse amplitude. The average pulse amplitude is computed from the IQ Meas trace. Only the locations where a pulse exists (-1 or 1 in IQ Ref) are included in the average.
See Also