STS Avg Power (802.15.4 HRP UWB)
is the RMS average power of the Scrambled Timestamp Sequence (STS), calculated over a resampled version of the input time data.
There are gaps between STS segments. The average power calculation includes these in the average.
See Also