STS Peak Power (802.15.4 HRP UWB)
is the power of the peak sample in the Scrambled Timestamp Sequence (STS), calculated over a resampled version of the input time data.
See Also
is the power of the peak sample in the Scrambled Timestamp Sequence (STS), calculated over a resampled version of the input time data.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |