Baseband Pulse Mask (802.15.4 HRP UWB)
shows the pulse shape from -3 ns to 5 ns and applies an upper and lower mask to the Real part of the data.
This trace is only applicable for channels with a pulse bandwidth of 499.2 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second..
If the trace does not initially display correctly, set the Trace Format to Real.
The Markers window displays the pass/fail status of the limit lines with 'X' and 'Y delta' information for each limit line segment.
Any part of the trace that fails the limit lines is drawn in red.
The data in this trace is unitless, being normalized to the value of the peak.
See Also