Status Tab (Licenses)

The Status tab on the Licenses dialog box provides information about the installed 89600 VSA software license.

License: Shows the license that is used to enable the 89600 VSA software if the license is valid. If the license is not valid, Demo appears in this field.

Version: Shows the current 89600 VSA software license version number.

Expiration: Shows either the current license expiration date for time-limited (perishable) licenses or shows Permanent for perpetual licenses.

Location: Shows Local for Demo, Trial, and Transportable licenses or, for Floating license installations, the floating license server's IP Internet Protocol: A set of instructions defining how information is handled as it travels between systems across the Internet. address. Local licenses are installed on the same PC as the VSA software is running.

Minimum License Version Required: Shows the minimum license version number required to run the currently installed 89600 VSA software release. A valid licensed 89600 VSA software requires that the Version license number must be greater than or equal to the Minimum License Version Required license number. If your option 200 license version number is less than the Minimum License Version Required number, the Demo license will be used.

Keysight Software Manager Utility: Opens the Keysight Software Manager Utility, which is used to easily manage your 89600 VSA software and option licenses.

The VSA software has integrated floating license check-out/check-in functionality. See Checking Out a Floating License for more information.

See Also

License Dialog Box